Solution


Haywire Twist Testing

Farmers may experience issues when it comes to their cattle fence on their ranch. If fencing becomes loose, livestock may escape or cause further damage. A farmer is seeking a force test on their twisted haywire of their fencing to see how durable it is from daily stress of their livestock.


HaywireTest Graphic

Summary

  • Customer Need / Challenge

    Farmers may experience issues when it comes to their cattle fence on their ranch. If fencing becomes loose, livestock may escape or cause further damage. A farmer is seeking a force test on their  twisted haywire of their fencing to see how durable it is from daily stress of their livestock.

  • Interface Solution

    Interface suggests installing the SSMF Fatigue Rated S-Type Load Cell in the test frame. The SSMF measures and monitors the force of the twisted haywire being tested. The results will be captured by the WTS-AM-1E and transmitted to the customer’s PC using the WTS-BS-6 Wireless Telemetry Dongle Base Station.

  • Results

    The customer was able to monitor the forces the twisted haywire could withstand.

Materials


  • SSMF Fatigue Rated S-Type

  • WTS-AM-1E Wireless Strain Bridge Transmitter Modules with Log100 software

  • WTS-BS-6 Wireless Telemetry Dongle Base Station

  • Customer haywire twisting test frame

  • Customer PC or Laptop

How it Works


  1. The  SSMF Fatigue Rated S-Type is installed into the test frame. The SSMF measures and monitors the amount of force that the of the twisted haywire can withstand

  2. Results are captured when connected to the WTS-AM-1E Wireless Strain Bridge Transmitter, and wirelessly transmitted to the customer’s PC using the WTS-BS-6 Wireless Telemetry Dongle Base Station with supplied Log100 software.

Download PDF